Hello Team,
I am using the external XDS110 debugger on the J7 TDA4V EVM with Virtualbox 6.1 running Ubuntu 18.04. The EVM is in No boot mode and i am able to load the launch scripts.Then, i try to load the binaries or when i try to run the default sciserver application on MCU1_0 core, the below error message pops up and i am not able to proceed further.This issue is always reproducible and it does not gets resolved.
I am unable to understand the root cause of the issue.
As a backup plan, i have installed CCS on windows environment, the same EVM with the XDS110 debugger works seamlessly.
Kindly let me know how to resolve this issue.