Part Number: TMS320C6745
Hi Team,
Our customer encountered some errors when he created a CCS project with bios. Then I shared the FAQ in the links below which help resolved the errors. However, another error appeared below.
Now I have project with bios base on generic c674x device and its pass the build.
But when I update to my device c6745 build fail with error message:
"configPkg/linker.cmd", line 26: error #10264: IROM memory range overlaps existing memory range SHDSPL2ROM
"configPkg/linker.cmd", line 27: error #10264: IRAM memory range overlaps existing memory range SHDSPL2RAM
"configPkg/linker.cmd", line 29: error #10264: DDR memory range overlaps existing memory range EMIFBSDRAM
error #10010: errors encountered during linking; "healium_medical_2.out" not built
My configPkg/linker.cmd is:
MEMORY
{
IROM (RX) : org = 0x11700000, len = 0x100000
IRAM (RWX) : org = 0x11800000, len = 0x40000
L3_CBA_RAM (RWX) : org = 0x80000000, len = 0x20000
DDR : org = 0xc3000000, len = 0x1000000
}
The C6745.cmd file is attached.
I guess we need to update the Memory region to the new device c6745 instead of generic c674x.
Can you please help with this issue?
Regards,
Danilo