This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
we have accomplished the LPDDR4 simulation. it was done by hyperlynx. we find that the LPDDR4_DQ17 have the max crosstalk of 68mV. all DDR routings are reused from TI reference design "PROC118E1_BRD.brd" per to TI requirement. we check the wolong design and "PROC118E1_BRD.brd" design and we find out that the LPDDR4_DQ17 routing may cause the LPDDR4_DQ17 high crosstalk problem. the attachment is the wolong roLPDDR4 SI Simulation Report_20221028_V3.01.pdfuting, the "PROC118E1_BRD.brd" routing and the simulation report. please help to confirm the following issues. 1) is 68mv crosstalk suitable with TDA4 VL requirements? 2) "PROC118E1_BRD.brd" has the same routing , what is the TDA4VL verification status? does the high crosstalk have any negative influence or is it OK per the the PROC118E1 testing and verification result?
As stated in other thread, TI does not measure crosstalk specifically (stand-alone). Crosstalk of the signal(s) is included as part of the overall JEDEC eye mask simulation. I will refer to another resource to respond on the status of testing/verification of the PROC118 design. Note the validation was/is likely not done on version E1 of the design, but a later version. We can also confirm the EVM version used during validation.
hi robert,
tks much for the information.
1. i have checked the LPDDR4_DQ17 routing both in E1 and E3 design. it sounds like the same routing design. i will compare the whole ddr routing in E1 and E3 later. so, please help to provide the DDR testing/verification information of the PROC118 design. we may reach a rudimentary conclusion if there is any risk.
2. is there any more action can i take to check this issue? if we ask the simulation engineer to channel sim LPDDR4_DQ17 in 3D-EM solver, does it will help us to check if it is OK? please help to provide some comments about it.
tks.
Hi,
Which DDR sub-system are you simulating? DDRSS0 or DDRSS1?
Regards,
Kevin
Note the bit in question is DQ17 of DDRSS0. Below is TI's simulation results from the EVM for byte lane 2 (which includes DQ17). Again - I do not have crosstalk specific information for DQ17, but rather the overall simulation results for Byte Lane 2.
Test | Total EW Margin (ps) | Total EH Margin (mV) | P-P VDDQ Noise (mV) |
DDR0 Byte2 Read at Pad | 7.36 | 12.72 | 10.46 |
DDR0 Byte2 Write at Pad | 39.66 | 100.04 | 206.84 |
Test | Total EW Margin (ps) | Total EH Margin (mV) | Vix DQS Ratio (%) |
DDR0 Byte2 Write at Pin | 49.96 | 60.96 | 13.29 |
Robert and kevin,
tks for the comments.
1. the EVM Byte lane 2 simulation result sound good. is byte lane 2 performance the worst comparing to the other bytes simulation result?
2. please help to share the status of testing/verification of the PROC118 design.
3. is there any more action can i take to check this issue? if we ask the simulation engineer to channel sim LPDDR4_DQ17 in 3D-EM solver, does it will provide more help? please help to provide some comments about it.