Hi,
Since there is no answer in the related question, is it possible to answer in a hurry?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Since there is no answer in the related question, is it possible to answer in a hurry?
Thanks,
Hi,
Are you referring below doc ?
https://software-dl.ti.com/processor-sdk-linux/esd/AM437X/08_02_00_24/exports/docs/linux/Overview.html
Best Regards
Ashwani
Hi,
Can you please provide SDK version you are working on ?
Best Regards
Ashwani
Hi, Ashwani
I plan to use the latest TI Linux SDK released to the web. ,
Thanks,
Eevee
Are you referring below doc ?
https://software-dl.ti.com/processor-sdk-linux/esd/AM437X/08_02_00_24/exports/docs/linux/Overview.html
Can you please confirm this as well ?
Best Regards
Ashwani
Hi, Ashwani
I checked the following, but there was no description of the information I was looking for.
Can you tell me about:
Regarding the IPv6 DHCP client, I would like to implement a function that allows IPv6 to be used in case IPv4 is exhausted in the future. Ideally, I would like to develop a device that implements software that uses the SDK for IPv4, and when that device is connected to an IPv6 network environment, I would like to have a configuration that can obtain an IPv6 address regardless of the router settings. Is it possible to get any advice to make it happen?
Thanks,
Eevee
Hi Eevee,
I think this is stack / application level changes / features (comes with kernel). It has nothing to do with driver layer (provided by TI).
Let me know how we can help you here ?
Best Regards
Ashwani
Hi, Ashwani
Is it correct to understand that it can be achieved by changing the application level?
It is currently in the concept stage and has not been worked out to the application.
Thanks,
Eevee
Is it correct to understand that it can be achieved by changing the application level?
As I already mentioned, it may be application or kernel level supported features / options to select.
Best Regards
Ashwani