This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please tell me about the following when not using DDR3SDRAM.
Device:TMS320C6678ACYP25
1. Can DDR pins be open(No Connect)?
2. Can DDRCLK(66MHz) pin be open?
3. Must DVDD15 and AVDDA2 be supplying power?
To Team, Please answer this question. It is taking 10 days
Daisuke,
There is the following application note, but I didn't see anything specifically addressing this question in section 6.1.1. Will forward this question internally.
https://www.ti.com/lit/pdf/sprabi1
Regards,
Kevin
Kevin, Thank you for your replay, Customer need to fix the circuit Design ASAP and need to clear this pending items. Could you answer it within today/tomorrow?
The data manual states if clock is unused it must be held at static state by pulling N leg to GND and P leg to VDD (for that specific IO). Yes all power rails are required to have proper voltage and sequence applied.
Robert, Thanls for answer. I design as below:
1. Can DDR pins be open(No Connect)?
open except to clock pins ans power pins.
2. Can DDRCLK(66MHz) pin be open?
pulling N leg to GND and P leg to VDD
3. Must DVDD15 and AVDDA2 be supplying power?
supplying power and applying power sequence
I recommended also connecting unused DQS/DQSn pins to pullup/down resistors (similar to DDRCLK). Other DDR pins can be left open.