Hi Experts,
I use TMS320C6655 with a single DDR3 4Gb (256M x 16). By using DDR3 Design Req for Keystone devices documentation, I noticed that I need to create 4 Net classes groups as below:
- SLRATE0,1 and DDRRESETn are not mentioned above, should they be in the control group or not in any group at all?
- Trace Width of 50-Ohm okay for them??
- Is spacing of 2W for Reset and 1.25W for SLRATE0,1 okay for them?
- Also, what trace Width and spacing that should I define for all Control groups if I'm not using Fly-by topology? (single DDR3 connected to DSP DDR controller)
- For all other non-differential signals (such as Address, Data, CASn, RASn, etc.) should I add 50ohm to the nets (close to the DDR3 side)?
- In the Data Net class, I noticed it's divided into Byte Lanes. But if I'm using only a single DDR3 (Data bus DDRA00-15 from DSP DDR controller to DDR3), do I need to separate the data net class into two classes, as described below or I can keep it a single Net class?
- For the Address Net class, what is the Trace wide and Spacing that is required if I use only a single DDR3 without Fly-by topology?