This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
flollow case:
I port
examples\drivers\mcan\mcan_loopback_interrupt\am62ax-sk\mcu-r5fss0-0_freertos
to the
examples\drivers\ipc\ipc_rpmsg_echo_linux\am62ax-sk\mcu-r5fss0-0_freertos
in this way ,I can debug the can,debug use can1 ,the pinmux is right ,but I find I can't no receive data from can box
root@am62axx-evm:/opt/edgeai-gst-apps# devmem2 0x0408403C /dev/mem opened. Memory mapped at address 0xffff9954b000. Read at address 0x0408403C (0xffff9954b03c): 0x00010000 root@am62axx-evm:/opt/edgeai-gst-apps# devmem2 0x04084040 /dev/mem opened. Memory mapped at address 0xffff8ef1f000. Read at address 0x04084040 (0xffff8ef1f040): 0x00050000 root@am62axx-evm:/opt/edgeai-gst-apps#
the mcan_loopback_interrupt_main code is :
void ipc_rpmsg_echo_main(void *args); void mcan_loopback_interrupt_main(void *args); void freertos_main(void *args) { mcan_loopback_interrupt_main(NULL); ipc_rpmsg_echo_main(NULL); vTaskDelete(NULL); }
/* * Copyright (C) 2021 Texas Instruments Incorporated * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* This example demonstrates the CAN message transmission and reception in * digital loop back mode with the following configuration. * * CAN FD Message Format. * Message ID Type is Standard, Msg Id 0xC0. * MCAN is configured in Interrupt Mode. * MCAN Interrupt Line Number 0. * Arbitration Bit Rate 1Mbps. * Data Bit Rate 5Mbps. * Buffer mode is used for Tx and RX to store message in message RAM. * * Message is transmitted and received back internally using internal loopback * mode. When the received message id and the data matches with the transmitted * one, then the example is completed. * */ #include <stdio.h> #include <kernel/dpl/DebugP.h> #include <kernel/dpl/AddrTranslateP.h> #include <kernel/dpl/SemaphoreP.h> #include <drivers/mcan.h> #include "ti_drivers_config.h" #include "ti_drivers_open_close.h" #include "ti_board_open_close.h" #define APP_MCAN_BASE_ADDR (CONFIG_MCAN0_BASE_ADDR) #define APP_MCAN_INTR_NUM (CONFIG_MCAN0_INTR) #define APP_MCAN_MSG_LOOP_COUNT (10U) /* Allocate Message RAM memory section to filter elements, buffers, FIFO */ /* Maximum STD Filter Element can be configured is 128 */ #define APP_MCAN_STD_ID_FILTER_CNT (1U) /* Maximum EXT Filter Element can be configured is 64 */ #define APP_MCAN_EXT_ID_FILTER_CNT (0U) /* Maximum TX Buffer + TX FIFO, combined can be configured is 32 */ #define APP_MCAN_TX_BUFF_CNT (1U) #define APP_MCAN_TX_FIFO_CNT (0U) /* Maximum TX Event FIFO can be configured is 32 */ #define APP_MCAN_TX_EVENT_FIFO_CNT (0U) /* Maximum RX FIFO 0 can be configured is 64 */ #define APP_MCAN_FIFO_0_CNT (0U) /* Maximum RX FIFO 1 can be configured is 64 and * rest of the memory is allocated to RX buffer which is again of max size 64 */ #define APP_MCAN_FIFO_1_CNT (0U) /* Standard Id configured in this app */ #define APP_MCAN_STD_ID (0xC0U) #define APP_MCAN_STD_ID_MASK (0x7FFU) #define APP_MCAN_STD_ID_SHIFT (18U) #define APP_MCAN_EXT_ID_MASK (0x1FFFFFFFU) /* In the CAN FD format, the Data length coding differs from the standard CAN. * In case of standard CAN it is 8 bytes */ static const uint8_t gMcanDataSize[16U] = {0U, 1U, 2U, 3U, 4U, 5U, 6U, 7U, 8U, 12U, 16U, 20U, 24U, 32U, 48U, 64U}; /* Semaphore to indicate transfer completion */ static SemaphoreP_Object gMcanTxDoneSem, gMcanRxDoneSem; static HwiP_Object gMcanHwiObject; static uint32_t gMcanBaseAddr; /* Static Function Declarations */ static void App_mcanIntrISR(void *arg); static void App_mcanConfig(Bool enableInternalLpbk); static void App_mcanInitMsgRamConfigParams( MCAN_MsgRAMConfigParams *msgRAMConfigParams); static void App_mcanEnableIntr(void); static void App_mcanConfigTxMsg(MCAN_TxBufElement *txMsg); static void App_mcanCompareMsg(MCAN_TxBufElement *txMsg, MCAN_RxBufElement *rxMsg); static void App_mcanInitStdFilterElemParams( MCAN_StdMsgIDFilterElement *stdFiltElem, uint32_t bufNum); void mcan_loopback_interrupt_main(void *args) { int32_t status = SystemP_SUCCESS; HwiP_Params hwiPrms; MCAN_TxBufElement txMsg; #if 0 MCAN_ProtocolStatus protStatus; #endif MCAN_RxBufElement rxMsg; MCAN_RxNewDataStatus newDataStatus; MCAN_ErrCntStatus errCounter; uint32_t i, bufNum, fifoNum, bitPos = 0U; /* Open drivers to open the UART driver for console */ Drivers_open(); Board_driversOpen(); DebugP_log("[MCAN] Loopback Interrupt mode, application started ...\r\n"); /* Construct Tx/Rx Semaphore objects */ status = SemaphoreP_constructBinary(&gMcanTxDoneSem, 0); DebugP_assert(SystemP_SUCCESS == status); status = SemaphoreP_constructBinary(&gMcanRxDoneSem, 0); DebugP_assert(SystemP_SUCCESS == status); /* Register interrupt */ HwiP_Params_init(&hwiPrms); hwiPrms.intNum = APP_MCAN_INTR_NUM; hwiPrms.callback = &App_mcanIntrISR; status = HwiP_construct(&gMcanHwiObject, &hwiPrms); DebugP_assert(status == SystemP_SUCCESS); /* Assign MCAN instance address */ gMcanBaseAddr = (uint32_t) AddrTranslateP_getLocalAddr(APP_MCAN_BASE_ADDR); /* Configure MCAN module, Enable LoopBack Mode */ App_mcanConfig(TRUE); /* Enable Interrupts */ App_mcanEnableIntr(); MCAN_BitTimingParams configParams; MCAN_getBitTime(APP_MCAN_BASE_ADDR,&configParams); DebugP_log("configParams %d %d %d %d %d %d %d %d!!\r\n", configParams.nomSynchJumpWidth, configParams.nomTimeSeg2, configParams.nomTimeSeg1, configParams.nomRatePrescalar, configParams.dataSynchJumpWidth, configParams.dataTimeSeg2, configParams.dataTimeSeg1, configParams.dataRatePrescalar ); /* Transmit And Receive Message */ for (i = 0U; i < APP_MCAN_MSG_LOOP_COUNT; i++) { #if 0 /* Configure Tx Msg to transmit */ App_mcanConfigTxMsg(&txMsg); /* Select buffer number, 32 buffers available */ bufNum = 0U; /* Enable Transmission interrupt for the selected buf num, * If FIFO is used, then need to send FIFO start index until FIFO count */ status = MCAN_txBufTransIntrEnable(gMcanBaseAddr, bufNum, (uint32_t)TRUE); DebugP_assert(status == CSL_PASS); /* Write message to Msg RAM */ MCAN_writeMsgRam(gMcanBaseAddr, MCAN_MEM_TYPE_BUF, bufNum, &txMsg); /* Add request for transmission, This function will trigger transmission */ status = MCAN_txBufAddReq(gMcanBaseAddr, bufNum); DebugP_assert(status == CSL_PASS); /* Wait for Tx completion */ SemaphoreP_pend(&gMcanTxDoneSem, SystemP_WAIT_FOREVER); MCAN_getProtocolStatus(gMcanBaseAddr, &protStatus); /* Checking for Tx Errors */ if (((MCAN_ERR_CODE_NO_ERROR != protStatus.lastErrCode) || (MCAN_ERR_CODE_NO_CHANGE != protStatus.lastErrCode)) && ((MCAN_ERR_CODE_NO_ERROR != protStatus.dlec) || (MCAN_ERR_CODE_NO_CHANGE != protStatus.dlec)) && (0U != protStatus.pxe)) { DebugP_assert(FALSE); } #endif DebugP_log("[MCAN] Wait for Rx 1completion, application started ...\r\n"); /* Wait for Rx completion */ SemaphoreP_pend(&gMcanRxDoneSem, SystemP_WAIT_FOREVER); DebugP_log("[MCAN] Wait for Rx 2completion, application started ...\r\n"); /* Checking for Rx Errors */ MCAN_getErrCounters(gMcanBaseAddr, &errCounter); DebugP_assert((0U == errCounter.recErrCnt) && (0U == errCounter.canErrLogCnt)); /* Get the new data staus, indicates buffer num which received message */ MCAN_getNewDataStatus(gMcanBaseAddr, &newDataStatus); MCAN_clearNewDataStatus(gMcanBaseAddr, &newDataStatus); /* Select buffer and fifo number, Buffer is used in this app */ bufNum = 0U; fifoNum = MCAN_RX_FIFO_NUM_0; bitPos = (1U << bufNum); if (bitPos == (newDataStatus.statusLow & bitPos)) { MCAN_readMsgRam(gMcanBaseAddr, MCAN_MEM_TYPE_BUF, bufNum, fifoNum, &rxMsg); } else { DebugP_assert(FALSE); } /* Compare Tx/Rx data */ App_mcanCompareMsg(&txMsg, &rxMsg); } /* De-Construct Tx/Rx Semaphore objects */ HwiP_destruct(&gMcanHwiObject); SemaphoreP_destruct(&gMcanTxDoneSem); SemaphoreP_destruct(&gMcanRxDoneSem); DebugP_log("All tests have passed!!\r\n"); Board_driversClose(); Drivers_close(); return; } static void App_mcanConfig(Bool enableInternalLpbk) { MCAN_StdMsgIDFilterElement stdFiltElem[APP_MCAN_STD_ID_FILTER_CNT] = {0U}; MCAN_InitParams initParams = {0U}; MCAN_ConfigParams configParams = {0U}; MCAN_MsgRAMConfigParams msgRAMConfigParams = {0U}; MCAN_BitTimingParams bitTimes = {0U}; uint32_t i; /* Initialize MCAN module initParams */ MCAN_initOperModeParams(&initParams); /* CAN FD Mode and Bit Rate Switch Enabled */ initParams.fdMode = TRUE; initParams.brsEnable = TRUE; /* Initialize MCAN module Global Filter Params */ MCAN_initGlobalFilterConfigParams(&configParams); /* Initialize MCAN module Bit Time Params */ /* Configuring default 1Mbps and 5Mbps as nominal and data bit-rate resp */ MCAN_initSetBitTimeParams(&bitTimes); /* Initialize MCAN module Message Ram Params */ App_mcanInitMsgRamConfigParams(&msgRAMConfigParams); /* Initialize Filter element to receive msg, should be same as tx msg id */ for (i = 0U; i < APP_MCAN_STD_ID_FILTER_CNT; i++) { App_mcanInitStdFilterElemParams(&stdFiltElem[i], i); } /* wait for memory initialization to happen */ while (FALSE == MCAN_isMemInitDone(gMcanBaseAddr)) {} /* Put MCAN in SW initialization mode */ MCAN_setOpMode(gMcanBaseAddr, MCAN_OPERATION_MODE_SW_INIT); while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(gMcanBaseAddr)) {} /* Initialize MCAN module */ MCAN_init(gMcanBaseAddr, &initParams); /* Configure MCAN module Gloabal Filter */ MCAN_config(gMcanBaseAddr, &configParams); /* Configure Bit timings */ MCAN_setBitTime(gMcanBaseAddr, &bitTimes); /* Configure Message RAM Sections */ MCAN_msgRAMConfig(gMcanBaseAddr, &msgRAMConfigParams); /* Set Extended ID Mask */ MCAN_setExtIDAndMask(gMcanBaseAddr, APP_MCAN_EXT_ID_MASK); /* Configure Standard ID filter element */ for (i = 0U; i < APP_MCAN_STD_ID_FILTER_CNT; i++) { MCAN_addStdMsgIDFilter(gMcanBaseAddr, i, &stdFiltElem[i]); } /* if (TRUE == enableInternalLpbk) { MCAN_lpbkModeEnable(gMcanBaseAddr, MCAN_LPBK_MODE_INTERNAL, TRUE); }*/ /* Take MCAN out of the SW initialization mode */ MCAN_setOpMode(gMcanBaseAddr, MCAN_OPERATION_MODE_NORMAL); while (MCAN_OPERATION_MODE_NORMAL != MCAN_getOpMode(gMcanBaseAddr)) {} return; } static void App_mcanConfigTxMsg(MCAN_TxBufElement *txMsg) { uint32_t i; /* Initialize message to transmit */ MCAN_initTxBufElement(txMsg); /* Standard message identifier 11 bit, stored into ID[28-18] */ txMsg->id = ((APP_MCAN_STD_ID & MCAN_STD_ID_MASK) << MCAN_STD_ID_SHIFT); txMsg->dlc = MCAN_DATA_SIZE_64BYTES; /* Payload size is 64 bytes */ txMsg->fdf = TRUE; /* CAN FD Frame Format */ txMsg->xtd = FALSE; /* Extended id not configured */ for (i = 0U; i < gMcanDataSize[MCAN_DATA_SIZE_64BYTES]; i++) { txMsg->data[i] = i; } return; } static void App_mcanInitStdFilterElemParams(MCAN_StdMsgIDFilterElement *stdFiltElem, uint32_t bufNum) { /* sfid1 defines the ID of the standard message to be stored. */ stdFiltElem->sfid1 = APP_MCAN_STD_ID; /* As buffer mode is selected, sfid2 should be bufNum[0 - 63] */ stdFiltElem->sfid2 = bufNum; /* Store message in buffer */ stdFiltElem->sfec = MCAN_STD_FILT_ELEM_BUFFER; /* Below configuration is ignored if message is stored in buffer */ stdFiltElem->sft = MCAN_STD_FILT_TYPE_RANGE; return; } static void App_mcanEnableIntr(void) { MCAN_enableIntr(gMcanBaseAddr, MCAN_INTR_MASK_ALL, (uint32_t)TRUE); MCAN_enableIntr(gMcanBaseAddr, MCAN_INTR_SRC_RES_ADDR_ACCESS, (uint32_t)FALSE); /* Select Interrupt Line 0 */ MCAN_selectIntrLine(gMcanBaseAddr, MCAN_INTR_MASK_ALL, MCAN_INTR_LINE_NUM_0); /* Enable Interrupt Line */ MCAN_enableIntrLine(gMcanBaseAddr, MCAN_INTR_LINE_NUM_0, (uint32_t)TRUE); return; } static void App_mcanInitMsgRamConfigParams(MCAN_MsgRAMConfigParams *msgRAMConfigParams) { int32_t status; MCAN_initMsgRamConfigParams(msgRAMConfigParams); /* Configure the user required msg ram params */ msgRAMConfigParams->lss = APP_MCAN_STD_ID_FILTER_CNT; msgRAMConfigParams->lse = APP_MCAN_EXT_ID_FILTER_CNT; msgRAMConfigParams->txBufCnt = APP_MCAN_TX_BUFF_CNT; msgRAMConfigParams->txFIFOCnt = APP_MCAN_TX_FIFO_CNT; /* Buffer/FIFO mode is selected */ msgRAMConfigParams->txBufMode = MCAN_TX_MEM_TYPE_BUF; msgRAMConfigParams->txEventFIFOCnt = APP_MCAN_TX_EVENT_FIFO_CNT; msgRAMConfigParams->rxFIFO0Cnt = APP_MCAN_FIFO_0_CNT; msgRAMConfigParams->rxFIFO1Cnt = APP_MCAN_FIFO_1_CNT; /* FIFO blocking mode is selected */ msgRAMConfigParams->rxFIFO0OpMode = MCAN_RX_FIFO_OPERATION_MODE_BLOCKING; msgRAMConfigParams->rxFIFO1OpMode = MCAN_RX_FIFO_OPERATION_MODE_BLOCKING; status = MCAN_calcMsgRamParamsStartAddr(msgRAMConfigParams); DebugP_assert(status == CSL_PASS); return; } static void App_mcanCompareMsg(MCAN_TxBufElement *txMsg, MCAN_RxBufElement *rxMsg) { uint32_t i; if (((txMsg->id >> APP_MCAN_STD_ID_SHIFT) & APP_MCAN_STD_ID_MASK) == ((rxMsg->id >> APP_MCAN_STD_ID_SHIFT) & APP_MCAN_STD_ID_MASK)) { for (i = 0U; i < gMcanDataSize[MCAN_DATA_SIZE_64BYTES]; i++) { if (txMsg->data[i] != rxMsg->data[i]) { DebugP_logError("Data mismatch !!!\r\n"); DebugP_assert(FALSE); } } } else { DebugP_logError("Message ID mismatch !!!\r\n"); DebugP_assert(FALSE); } return; } static void App_mcanIntrISR(void *arg) { uint32_t intrStatus; intrStatus = MCAN_getIntrStatus(gMcanBaseAddr); MCAN_clearIntrStatus(gMcanBaseAddr, intrStatus); DebugP_logError("App_mcanIntrISR !!!\r\n"); if (MCAN_INTR_SRC_TRANS_COMPLETE == (intrStatus & MCAN_INTR_SRC_TRANS_COMPLETE)) { SemaphoreP_post(&gMcanTxDoneSem); } /* If FIFO0/FIFO1 is used, then MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG macro * needs to be replaced by MCAN_INTR_SRC_RX_FIFO0_NEW_MSG/ * MCAN_INTR_SRC_RX_FIFO1_NEW_MSG respectively */ if (MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG == (intrStatus & MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG)) { SemaphoreP_post(&gMcanRxDoneSem); } return; }
when I send data to mcan(soc),the can box notify send fail,so the can has problem
and isr has no irq update
[MCAN] Loopback Interrupt mode, application started ... configParams 0 2 5 7 0 2 3 1!! [MCAN] Wait for Rx 1completion, application started ...
You can see my code for more details
/* if (TRUE == enableInternalLpbk) { MCAN_lpbkModeEnable(gMcanBaseAddr, MCAN_LPBK_MODE_INTERNAL, TRUE); }*/
Hi,
Could you describe more about the hardware setup you have, and pins connected?
To test MCAN on AM62A SK, we use the CAN-FD controller on the AM62A and 1x external CAN transceiver, which completes one node on the CAN bus. Connect the CAN transceiver to AM62A as shown in the following diagram:
Then, the MCAN_H and MCAN_L pins from transceiver can be connected to CAN-to-USB connector to send/receive data via PC.
Regards,
Aparna
Hi,
The code changes made in mcan_loopback_interrupt.c looks correct.
Please check the following:
1) Probe the pins to eliminate any hardware related faults.
2) Make sure the MCU_MCAN instance used is the same as set in syscfg.
Regards,
Aparna
1: I think There's no problem with the peripheral circuit
for rx,I can receive signal for PC can box,
2.about pinmux,I add print ,it is ok
the adapter address is right ,I use mcu mcan1
#define APP_MCAN_BASE_ADDR (CONFIG_MCAN1_BASE_ADDR)
#define APP_MCAN_INTR_NUM (CONFIG_MCAN1_INTR)
#define CONFIG_MCAN1_BASE_ADDR (CSL_MCU_MCAN1_MSGMEM_RAM_BASE)
#define CONFIG_MCAN1_INTR (46U)
#define CSL_MCU_MCAN1_MSGMEM_RAM_BASE (0x4e10000UL)
1: I think There's no problem with the peripheral circuit
for rx,I can receive signal for PC can box,
2.about pinmux,I add print ,it is ok
the adapter address is right ,I use mcu mcan1
#define APP_MCAN_BASE_ADDR (CONFIG_MCAN1_BASE_ADDR)
#define APP_MCAN_INTR_NUM (CONFIG_MCAN1_INTR)
#define CONFIG_MCAN1_BASE_ADDR (CSL_MCU_MCAN1_MSGMEM_RAM_BASE)
#define CONFIG_MCAN1_INTR (46U)
#define CSL_MCU_MCAN1_MSGMEM_RAM_BASE (0x4e10000UL)
Last update:
when canbox PC send canfd data to board,It has isr ,I print isr status
my settings on can box is right?
Hi,
The MCAN config template file didn't contain the code to convert the decimal value to hex value. Please update the mcan_config.c.xdt file with the below code.
%%{ let module = system.modules['/drivers/mcan/mcan']; %%} /* * MCAN */ /* MCASP Default Bit timing Parameters */ MCAN_BitTimingParams gMcanBitTimingDefaultParams = { .nomRatePrescalar = 0x`module.$static.nomRatePrescalar.toString(16).toUpperCase()`U, .nomTimeSeg1 = 0x`module.$static.nomTimeSeg1.toString(16).toUpperCase()`U, .nomTimeSeg2 = 0x`module.$static.nomTimeSeg2.toString(16).toUpperCase()`U, .nomSynchJumpWidth = 0x`module.$static.nomSynchJumpWidth.toString(16).toUpperCase()`U, .dataRatePrescalar = 0x`module.$static.dataRatePrescalar.toString(16).toUpperCase()`U, .dataTimeSeg1 = 0x`module.$static.dataTimeSeg1.toString(16).toUpperCase()`U, .dataTimeSeg2 = 0x`module.$static.dataTimeSeg2.toString(16).toUpperCase()`U, .dataSynchJumpWidth = 0x`module.$static.dataSynchJumpWidth.toString(16).toUpperCase()`U, };
The mcan_config.c.xdt file is located at path {MCU+SDK}/source/drivers/.meta/mcan/templates. After updating the file restart the sysconfig tool and it will work fine.
Please let me know if this solution works for you.
Regards,
Aparna
update mcan_config.c.xdt to {MCU+SDK}/source/drivers/.meta/mcan/templates/mcan_config.c.xdt
the make -j,update mcu_plus_sdk_am62ax_08_06_00_18\examples\drivers\ipc\ipc_rpmsg_echo_linux\am62ax-sk\mcu-r5fss0-0_freertos\ti-arm-clang\am62a-mcu-r5f0_0-fw to /lib/firmware/pdk-ipc/am62a-mcu-r5f0_0-fw
on therside,I print the paramter of can
Hi,
Any updates on this issue?
Have you been able to solve it or need any assistance?
Regards,
Aparna
Hi,
Sorry to hear that!
There is less clarity as to why external MCAN connection is not established here.
I will update you if there is any related information.
Regards,
Aparna
Hi,
I have tested the external loopback example (with a different transceiver device), and after a few modifications of this example:
examples\drivers\mcan\mcan_loopback_interrupt\am62ax-sk\mcu-r5fss0-0_freertos
it works for me.
I have used MCU_MCAN0 instance to test MCAN in external loopback setup. I have set MCAN bit timing parameters (bit rates and sampling points) correctly.
To calculate Sampling point, use this formula:
Sampling Point (%) = (1 + TSEG1) / (1 + TSEG1 + TSEG2)
Reference code:
5710.empty_am62ax-sk_mcu-r5fss0-0_freertos_ti-arm-clang.zip
Hardware setup image:
Output image:
Regards,
Aparna