Dear TI Forum,
I am looking for a checklist on how to modify an Industrial Communication SDK example running on MCU R5F / PRU core into a Linux Remote Proc firmware project that will initialize and load R5F example application.
My main dilemma is if/how to modify a device tree dts files (a short example) to perhaps disable PRU-ICSSG cores from being used by A53/Linux since the R5F will initialize and download the PRU Firmware?
I believe the below checklist should be sufficient to get it up and running:
1. I need to enable IPC into syscfg and maybe modify/add the UART for MCU debug messages.
2. Change the application's linker.cmd to adjust the mem for R5F from Linux dtsi "reserved-memory" setting.
3. Change the dts file to disable Uart and PRU something like:
&icssg0_mdio {status = "reserved";}; ???
&mcu_uart0 {status = "reserved";};
Any help would be much appreciated.
Thank you