Other Parts Discussed in Thread: TEST2
Hi experts,
We have started the procedure to swap the five GP variants that was wrongly mounted to HS variants. I will get the first two samples tomorrow. We have decided to go for UART boot in factory for the programming of OTP and hence we have rerouted mcu_uart0 to follow TI standard pinmux.
Until then, we have four questions:
- Is the OTP writing being done solely by uploading the keywriter-bin with the VPP_MCU voltage set to 1.8V? I.e. there is no need to further communicate with the keywriter application, other than getting the debug output for verification?
- What is written is a result of the settings in the x509-certificate in the keywriter-bin only. Is this correct?
- Is RSA4096 still the only supported variant for the hashes?
- Is it possible, using extended OTP, to change the VID, PID and serialnumber that is presented to the host at USB boot? We would like to use our own, so that our customers are not presented with a TI-product.
Regards,
/Bo