Is CanTrcv SN65HVD230 is compatible with AM62x MCU_MCAN0?

Other Parts Discussed in Thread: SN65HVD230, UNIFLASH, SYSCONFIG

Hi Nihar,

We are able to make Can_Init successful now.. but the issue is observed during transmitting the CAN frames.
We are able to receive only one frame on the PCAN and no other frames are observed.. MCU_MCAN0 is configured in INTERRUPT mode.
We are using MCU_MCAN0 and external Transceiver SN65HVD230 with below connections:

  • MCU_MCAN0_RX is brought out by pin 22 on MCU Header.
  • MCU_MCAN0_TX is brought out by pin 16 on MCU Header.

Could you please confirm if CanTrcv SN65HVD230 is compatible with AM62x MCU_MCAN0.

BR,
Shubham