Other Parts Discussed in Thread: DRA821
Tool/software:
Hi.
We connected the DRA821 PCI-e 4LANE to the PCI-e switch chip on our development board (custom board) as shown below.
However, only x1LANE is connected between DRA821 and PCI-e switch.
The attached file below contains Linux LSPCI information.
If you look at the lspci information of DRA821, it looks like it is set to 1lane. (But we have set it to 4LANE in DTS.)
and The PCI-E switch was downgraded and connected to 1LANE (This is evidence that the PCI-E switch is trying to operate in 4lane.)
When booting, I measured the waveform of each PCI-E LANE using a scope, but only LANE 0 showed the waveform.
There is no signal from other LANE (LANE1, 2, 3)
The attached file below is DTS information.
It's not clear. After all checks, it appears that there is a problem with the DRA821 settings.
Please review LSPCI log and DTS file why DRA821 and PCI-e switch cannot be connected via PCI-E 4LANE.