This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear TI-Support,
The LPDDR4 RAM is to be tested as part of a customer project.
As this does not have a test mode, testing via boundary scan is difficult. A test via software (e.g. a small baremetal program that can be loaded into the RAM via JTAG) would be more effective here.
Is there an example of a bare metal application for accessing the DDR RAM?
We saw that the board initialization via GEL scripts performs a lot of steps before being able to initialize the LPDDR4 RAM.
An example Cortex-R5 bootloader that does the hardware initialization would be very helpful.
Best regards,
Andreas
Hi,
Is there an example of a bare metal application for accessing the DDR RAM?
The short answer is no.
Accessing the DDR memory is performed directly by accessing the DDR memory address region of the TDA4 device (ex: write to address 0x80000000 and read it back).
We saw that the board initialization via GEL scripts performs a lot of steps before being able to initialize the LPDDR4 RAM.
An example Cortex-R5 bootloader that does the hardware initialization would be very helpful.
TI provides bootloader code through the Software Development Kits (SDKs). See for example the tiboot3.bin file which includes the R5 bootloader code to initialize DDR.
https://www.ti.com/tool/PROCESSOR-SDK-J721S2
Regards,
Kevin
Hi Kevin,
thanks for your reply. Our usecase is to transfer bootloader code into the OCM RAM of the Cortex-R5 and run it. Currently we had issues to finish the board initialization. This failed with the keywriter_img and flash_programming image (UNIFLASH Tool).
We know about the High-Level documentation, but we are missing details here, why the initialization does not finish (see my other tickets). It would be very helpful to have a step-by-step guide on how to compile a baremetal R5 application that does the board startup.
Best regards,
Andreas
Hi Andreas,
Currently we had issues to finish the board initialization. This failed with the keywriter_img and flash_programming image (UNIFLASH Tool).
If these comments are related to the original E2E below, let's please keep discussing the issue in the original E2E thread. Unfortunately, I am not the right TI employee to assist you with UNIFLASH.
Regards,
Kevin
Hi Kevin,
in that case I want to stay within the provided SDK boot code provided byti-processor-sdk-rtos-j721e-evm-10_00_00_05/pdk_jacinto_10_00_00_27
in packages/ti/boot/sbl
Running make help
in packages/ti/build
shows me that there are many sbl targets for mmcsd, ospi, uart as well as hs variants. For the SK-TDA4VM evaluation board I want to try running the sbl_uart_img
via the XDS200 TI Debugger and Code Composer Studio 12.4:
make BOARD=j721e_evm CORE=mcu1_0 all
(required due to missing dependencies)
make BOARD=j721e_evm CORE=mcu1_0 sbl_uart_img
loadJSFile("/home/dev/ti/ti-processor-sdk-rtos-j721e-evm-10_00_00_05/pdk_jacinto_10_00_00_27/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js")
MCU_Cortex_R5_0 > Load Code > /home/dev/ti/ti-processor-sdk-rtos-j721e-evm-10_00_00_05/pdk_jacinto_10_00_00_27/packages/ti/boot/sbl/binary/j721e_evm/uart/bin/sbl_uart_img_mcu1_0_relase.xer5f
sbl_boot_test
MCU_Cortex_R5_0 > Load Code >
/home/dev/ti/ti-processor-sdk-rtos-j721e-evm-10_00_00_05/pdk_jacinto_10_00_00_27/packages/ti/boot/sbl/example/k3MulticoreApp/binary/j721e/sbl_boot_test_j721e_evm_mcu1_0TestApp_release.xer5f
HwiP_undefined_handler_c()
keywriter_img
packages/ti/boot/keywriter/binary/keywriter_img_j721e_release.xer5f
main()
UART_printf()
. I think this is expected, as the function requires TISCI to be running (is this correct?)I am missing any starting point to correctly run the baremetal board initialization, so that we can adjust the code to run DDR tests.
Regards,
Andreas
Hi Kevin,
an addendum: apparently there is also a timing issue.
I can run the Cortex-R5 ELF packages/ti/boot/sbl/binary/j721e_evm/emmc_boot0/bin/sbl_emmc_boot0_img_mcu1_0_release.xer5f
when I connect and load the ELF to MCU1_0 directly after a reset.
Inside the sbl_main.c
I can see that we can enable the DDR initialization with -DSBL_ENABLE_DDR
, but the program fails at loading the SYSFW with SBLSciClientInit(devGroup)
, I guess due to the SBL being unable to read the sysfw image from emmc0, as it is currently empty.
Also the SBL_log()
output via UART1 cannot be deciphered. Is the baudrate configured to another value than 115200?
Regards,
Andreas
Hi Andreas ,
packages/ti/boot/sbl/binary/j721e_evm/emmc_boot0/bin/sbl_emmc_boot0_img_mcu1_0_release.xer5f
when I connect and load the ELF to MCU1_0 directly after a reset.
Are you executing this test according to 4.3 CCS/JTAG this procedure?
4.3 CCS/JTAG Apply attached patch as mentioned in faq-how-to-flash-ospi-using-ccs-on-tda4x-dra82-evm on PDK, which is available as part of PSDKRA. This patch adds a utility that can be used to flash OSPI using CCS and JTAG interface. 4.3.1 Flashing Instructions 1. Apply 0001-Add-support-for-flashing-OSPI-flash-using-CCS.patch on the PDK. 2. Change flag USE_CCS to yes in the pdk/packages/ti/board/utils/uniflash/target/build/uart_make.mk file. 3. Rebuild flash programmer by using make -sj PLATFORM=j721e_evm board_utils_uart_flash_programmer from pdk/packages/ti/build. 4. Flash Writer binary would be available in pdk/packages/ti/board/utils/uniflash/target/bin/j721e_evm/ uart_j721e_evm_flash_programmer_release.xer5f. 5. Launch CCS and target configuration. For details on this step, see this. 6. From Scripting Console run loadJsFile("pdk/packages/ti/drv/Sciclient/tools/ccsLoadDmsc/j721e/launch.js") from the CCS scripting console. 7. Once Java script is completed, load flash writer code in MCU_Cortex®_R5_0 core and Run it. 8. Application runs and displays 3 menu options on the CCS console, Erase OSPI flash, Flashing file in OSPI and exit. 9. For erasing flash, select the start address and size to be erased. 10. For flashing a file, enter the file name with the full path, then enter offset where file is to be flashed, then load the file using CCS scripting console (command to load is printed on CCS console). Once file is loaded from scripting console, enter '0' on CCS console. 11. Press '2' on main menu to exit, after all files are flashed.
Regards,
Karthik
Hi Karthik,
I remember following these exact flashing instructions, but I wasn't aware that the patch also should be applied to the latest SDKs (PSDK version 10). Best way would be to test this with PSDK version 7.3, but currently the PSDK download from TI fails/is slow. I resolved two compiler errors for `ccs_main.c` and was able to build the target `board_utils_uart_flash_programmer`.
After that I opened CCS, launched the target configuration and successfully ran the launch.js script:
Running the cortex-r5 elf uart_j721e_evm_flash_programmer_release.xer5f
did not succeed. Processor runs, but never gets to the main function. When halting the CPU, the PC is at address 0x4CA:
Loading the Cortex-R5 elf directly after reset (without running launch.js) was possible, but the program polls endlessly for the sciserver to respond (compare backtrace):
From my point of view this behaviour is expected, because the sciserver testapp is not running (it should be running on MCU_Cortex_R5_0 and I am using this core for the elf file).
Do you think this can be tested on a J721S2_HS device (with `make -j8 BOARD=j721s2_evm CORE=mcu1_0 board_utils_uart_flash_programmer_hs`)? I am not 100% sure, but SciClient is running on the SMS core for HS devices, right?
Edit: I tried running the board_utils_uart_flash_programmer_hs ELF on the J721S2 HS-FS variant and the MCU_CORTEX_R5_0 did not execute the ELF at all.
Regards,
Andreas
Hi Andreas,
Our usecase is to transfer bootloader code into the OCM RAM of the Cortex-R5 and run it
If transferring bootloaders is your use case, can you please try with SD boot mode. It would be simpler to start with that.
Currently we had issues to finish the board initialization. This failed with the keywriter_img and flash_programming image (UNIFLASH Tool).
Could you confirm whether you're using an HS or GP device?
Regards,
Karthik
Hi Karthik,
If transferring bootloaders is your use case, can you please try with SD boot mode. It would be simpler to start with that.
How do I correctly boot up the uart_j721e_evm_flash_programmer_release
? I guess I have to put the uart_j721e_evm_flash_programmer_release.tiimage
into the boot partition of the SD card instead of the .xer5f
is that correct?
I am not interested in booting via the default tiboot3.bin
, because we require a bare-metal emmc flashing application over JTAG
Could you confirm whether you're using an HS or GP device?
I am currently using a J721EXSKG01EVM (SK-TDA4VM) GP device and want to move on to a J721S2 HS Device when I have a working setup.
Best regards,
Andreas
Hi Andreas,
I am currently using a J721EXSKG01EVM (SK-TDA4VM) GP device and want to move on to a J721S2 HS Device when I have a working setup.
The SK-TDA4VM (Starter Kit) device does not have an eMMC. Please refer to the schematic. It seems like you are using the TDA4 Flashing Techniques document for the J721e_EVM device.
Regards,
Karthik
Hi Karthik,
I am aware of it, but the topic of this ticket is about Board and DDR initialization via bare-metal Cortex-R5 application. I just used the emmc0 sbl image, but the application aborted before even initializing the eMMC0.
A test on SK-TDA4VM (J721E_EVM) with ti-processor-sdk-rtos-j721e-evm-07_03_00_07
using sbl_uart_img
launch.js
script with loadSciserverFlag = 0
The next step could be to move the DDR Initialization before the SBL_SciClientInit(), but I am not sure if the SciClient is needed to initialize PLLs, Clocks and DDR. Do you know the required preconditions to perform the DDR initialization?
Best regards,
Andreas
Hi Andreas,
The rtos is not validated on the tda4vm-SK board. The validated SDK:
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-SK-TDA4VM/10.00.00.08
So if you have the sk EVM you can use the sd card as mentioned above by Karthik. We do not have a barmetal application that can be used to initialised DDR and even if that exists for EVM that's not validated on SK boards.
And yes the device manager is needed for any of the clock requests.
Best regards,
Keerthy
Hi Keerthy,
thanks for the answer, that's very helpful to know!
In that case do you know if the RTOS package can be used in combination with the XJ721S25AALZ (TDA4VE-HS)? The RTOS SDK Support will be required anyway in the near future for OTP Keywriting.
Best regards,
Andreas
Hi Keerthy,
one remark: With the insights from https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1418335/faq-j784s4xevm-how-to-load-tifs-using-jtag-on-hs-fs-device/5433552#5433552
I was able to test the SBL initialization, but it fails at the "Initializing DDR ..."-step and never prints "done". Do you know why this could happen?
Best regards,
Andreas
Hi Andreas,
step and never prints "done". Do you know why this could happen?
The relevant discussions is going on at this thread https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1420023/processor-sdk-j721s2-cannot-run-keywriter-via-jtag-xj721s25aalz-hs-fs-device , Please follow the thread above for further support .
Reagrds,
Karthik
Closing thread thread now that https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1420023/processor-sdk-j721s2-cannot-run-keywriter-via-jtag-xj721s25aalz-hs-fs-device is also closed.