This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We use DDR: MT53E2G32D4DE-046 AAT:C with DRA821U-Q1 which has DDRSS0 only
in the configuration Tools, Questions:
Thanks
Max
Hi Max,
We only need to set DDRSS0 values, ignore other DDRSS1-3 values, correct?
Correct. Note that the online (sysconfig) version will not even show inputs for DDRSS1-3 for DRA821.
Frequency Set0, Frequency Set 1 and Set 2 ? what is set 0, set1 and set 2? can we say set 0 min Frequency and set 1 max frequency?
FS0 is the boot frequency. This is typically 55 MHz or less.
FS1/FS2 should be set the same, and correspond to the operating frequency. Max value supported for DRA821 is 1600 MHz.
WL set A and WL set B? do I have to set A and B? what about just set A?
I am not clear on the question.
~~~~~~~~~~~~~~
As a small request - since this question is a follow-up to the existing thread, can you please use the existing thread(s) for follow-up questions as opposed to creating new tickets?
Thanks,
Kevin
I meant WLS options: WL SET A and WL SET B, which one should i choose ?currently it is WL set A for EVM.
Thanks
Max
If your memory datasheet and/or supplier does not indicate which write latency set to use, then I would suggest leaving it as set A.
Regards,
Kevin