Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi TI-Team,
some time ago we built a custom board with AM243x chip (Board A). We did a new revision of this board with a AM6442 chip (Board B).
On board B we now have problems to get OSPI boot running. On the new boards the exact same flash was used, which was successfully tested/used on the Board A in conjuction with AM243x. The assembled flash is a Micron MT35XU512ABA1G12-0AAT.
The OSPI flash in general is working. This means after booting in DEV-Boot mode and doing basic SOC init I can successfully execute programs using OSPI Flash such as OSPI Flash IO or OSPI Flash Diagnostic. I am also able to flash a bootloader via a modified JTAG uniflash program.
Here is the read JEDEC information:
{
"flashSize": 67108864,
"flashPageSize": 256,
"flashManfId": "0x2C",
"flashDeviceId": "0x5B1A",
"flashBlockSize": 131072,
"flashSectorSize": 4096,
"cmdBlockErase3B": "0xD8",
"cmdBlockErase4B": "0xDC",
"cmdSectorErase3B": "0x20",
"cmdSectorErase4B": "0x21",
"protos": {
"p111": {
"isDtr": false,
"cmdRd": "0x03",
"cmdWr": "0x02",
"modeClksCmd": 0,
"modeClksRd": 0,
"dummyClksCmd": 0,
"dummyClksRd": 0,
"enableType": "0",
"enableSeq": "0x00",
"dummyCfg": null,
"protoCfg": null,
"strDtrCfg": null
},
"p112": null,
"p114": null,
"p118": {
"isDtr": false,
"cmdRd": "0x7C",
"cmdWr": "0x84",
"modeClksCmd": 0,
"modeClksRd": 1,
"dummyClksCmd": 0,
"dummyClksRd": 7,
"enableType": "0",
"enableSeq": "0x00",
"dummyCfg": null,
"protoCfg": null,
"strDtrCfg": null
},
"p444s": null,
"p444d": null,
"p888s": null,
"p888d": {
"isDtr": false,
"cmdRd": "0x0B",
"cmdWr": "0x12",
"modeClksCmd": 0,
"modeClksRd": 0,
"dummyClksCmd": 8,
"dummyClksRd": 20,
"enableType": "0",
"enableSeq": "0x00",
"dummyCfg": {
"isAddrReg": false,
"cmdRegRd":"0x00",
"cmdRegWr":"0x00",
"cfgReg":"0x00000000",
"shift":0,
"mask":"0x00",
"bitP":0
},
"protoCfg": {
"isAddrReg": false,
"cmdRegRd": "0x00",
"cmdRegWr": "0x00",
"cfgReg": "0x00000000",
"shift": 0,
"mask": "0x00",
"bitP": 0
},
"strDtrCfg": {
"isAddrReg": false,
"cmdRegRd": "0x00",
"cmdRegWr": "0x00",
"cfgReg": "0x00000000",
"shift": 0,
"mask": "0x00",
"bitP": 0
}
},
"pCustom": {
"fxn": null
}
},
"addrByteSupport": "1",
"fourByteAddrEnSeq": "0xA1",
"cmdExtType": "REPEAT",
"resetType": "0x10",
"deviceBusyType": "0",
"cmdWren": "0x06",
"cmdRdsr": "0x05",
"srWip": 0,
"srWel": 0,
"cmdChipErase": "0xC7",
"rdIdSettings": {
"cmd": "0x9F",
"numBytes": 5,
"dummy4": 0,
"dummy8": 0
},
"xspiWipRdCmd": "0x00",
"xspiWipReg": "0x00000000",
"xspiWipBit": 0,
"flashDeviceBusyTimeout": 64000000,
"flashPageProgTimeout": 120
}
However, after booting I will not enter the SBL NULL bootloader and cannot see any messages print on debug UART.
I tried to debug SBL NULL by adding a `loop_forever()` directly in main. However, I will not be able to step into loop. Instead I see that I am stuck at "strange" addresses.


So for me it seems like ROM-code of chip is not able to successfully access OSPI Flash at boot time.
Do I have any further debugging possibilities?
Are there any registers etc. where I could find out what the problem is?
Thanks for any help or tips in advance!
Kind regards,
Dominik