Hello
We have a platform for with a Few C6678 which we would like to boot.
The Devices are connected to an Srio switch and are intended to work on 4x.
We would like to use spi boot to configure the 4x for srio and the Ddr,
and than boot the application through Srio.
Our Fpga will simulate an SPI FLASH for the boot purpose.
Questions we would need your help on:
- Is there a software demo or code for Srio boot using messaging.?!
The documentation is not clear enough to me -
- what does the end of boot packet mean ? how does it look?
is it just the end of the boot table?
in the message mode boot header what does block size=6 means?
is this header the data at the beginning of each srio message? why 6?
is this header a 32 bit ? how big is the block size field?
Do i have to add a checksum for each message?
- about Spi - do you have an example file of an spi boot parameter table for rebooting srio in 4x lanes?
- Another option is not to use Spi at all, to boot from Srio and than
through the switch send the command of moving to 4 lanes to all Dsp's,
what do you think about this option in term of feasibility, stability and boot speed.
does it seem to be a better option ?
Thanks