This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to boot my application to DDR3 through SPI BOOT with the Boot Config Table, but the ddr configuration values of our board diffrent from 6678EVM. I don't know how to modify the Boot Config Table of the APP IMAGE,i hope for your help! below is the ddrtable[120] in <AddDDrTable.exe> for 6678EVM:
0x00, 0x00, 0x00, 0x70, 0x00, 0x87, 0x35, 0x00, 0x02, 0x42, 0x80, 0xF5, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1C, 0x00, 0x00, 0x00, 0x02,
0x63, 0x06, 0x2A, 0x32, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x14, 0x50, 0x11, 0x13, 0x78, 0x3C, 0x30, 0x71, 0x7F, 0xE3, 0x55, 0x9F, 0x86, 0xAF,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x70, 0x07, 0x32, 0x14, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x01, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x03, 0x05
As the boot loader user guide suggests, the romparse utility was created to append boot parameter table and boot configuration table to the boot table. However in the current form the romparse is only used to append boot parameter tables. For DDR configurations you will need to create a pragma DATA_Section in your main function that places the DDR configuration table in the DDR config memory space. The boot loader copies this DDR configuration table when it loads the application binary and when it notices the change in the DDR configuration memory section it will proceed to initialize DDR before loading the DDR sections of your application binary.This is demonstrated in the .bat file included in the example attached.
Please look at the example attached. The parameter table in the nysh.spi.map provides the modified SPI boot parameter table. The spiboot.c file and spiboot.cmd demonstrates the placement of the DDR3 configuration table.