This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed

Other Parts Discussed in Thread: CCSTUDIO, TMDSICE3359, AM3359

Hello,

After I had spent lot of time to get the virualbox on my Windows 7 connected to the Internet, I was able to carry on "Processor SDK Linux Training: Hands on with the Linux SDK". However, I have got the following problems when Configuring Remote System Explorer (RSE).

1. "Check ssh.terminals to use Secure Shell to work with terminals." doesn't exist.

2. After configuring, I tried to "connect" and I got "Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed".


I don't think the first one is a real problem. However the second is a serious problem simply because I get stuck there. I can't remotely access the AM335x ICE V2 board and can't debug it either.

I searched the Internet for a solution but most of solutions are irrelevant. None of answers helps. Please tell me if the sftp server is not running on the Eval board. It doesn't look like a network problem since I can ping my am335x ICE V2 board.

Please advise.


Many thanks!