Hi,
We will be shortly working on the TDA2Ex ES2.0 GP EVM Vision Kit
1) we need one MIPI CSI2 camera to connect to the EVM vision kit and need TI’s suggestion. The MIPI CSI2 based camera sensor is planned to be connected to the CSI2 port of the EVM CPU board. We plan to use this sensor to develop and test the 8 bit extraction of CAL output which we will need in the final board(In the final board we are having 24bit mipi input and need to extract the 8 bit data from the 24 bit input e2e.ti.com/.../569557).
Preferably this MIPI CSI2 camera should have been already tested on the vayu evm board by TI.
2) Also we want to confirm the following path of the MIPI CSI2 driver source code (ti_components/drivers/starterware_01_07_00_19/vpslib/hal).
Is this the same driver which TI has tested for the MIPI CSI2 interface? (vision sdk 2.11 release)
3) Can we get more details from TI regarding the test setup used by TI for MIPI CSI2 interface testing on EVM vision kit(camera sensor used, part number etc).
4) We plan to use the spectrum digital deserialiser (703769-0001) and serialiser (703817-0001). Has this been tested on EVM vision kit by TI? In the vision sdk user guide for TDA2Ex only SV600964 board has been mentioned.
Thanks
Vijay
703769-0001 |