Part Number: AM5728
Other Parts Discussed in Thread: BEAGLEBOARD-X15, TLV320AIC3104, TLV320AIC3204, PCM3168A-Q1
Hello,
I need to output 8 audio channels (each receiver would be single channel; 2 wire; 600Ohm) from a AM5728.
I read on the documentation that:
"Audio Connectivity Peripherals
• Eight multichannel audio serial ports (McASP):
– Two McASP supporting up to 16 channels each and independent TX/RX clock/sync domains"
So it seems it is possible to transmit 8 different audio channels by using a single McASP interface.
I guess I need to connect 8 different audio CODECs to that McASP interface.
How is the connection done? Is it possible to cascade connect 8 CODECs to a single McASP interface?
What kind of external audio CODECs do I need?
Regards,