I have a question about DDRDRIVE[1:0]. It has two settings (high/low) in DDR2 mode to control output driver strength. It is also described as "output driver impedance". This makes sense because decreased drive strength is the same as increased output impedance.
My question is if there is either a) anything to quantify "high" and "low" drive strength or b) any practical guidelines regarding what trace geometries or trace impedances lend themselves to each setting. Is there any direct relationship between the value of the DDR_ZP resistor and drive strength?
I'm driving 4-mil traces whose characteristic impedance works out to around 50 ohms with no external termination, mostly just under 1 inch long. I'm almost sure I need to use low drive strength, but I just wanted to see if there's more info out there.
When I search the memory controller user's guide, I also find VTPIO_CTL[3..5] contains drive strength control bits. My understanding is that setting is not memory-controller specific and is not intended for user knob-twiddling in any case.