This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I would like to install the C6000 compiler ver.8.1.0.
I found but how do I install it offline?
Thanks,
KH
Installation details will always show the latest version of a feature that is installed. In this case the latest version of the 8.1 compiler installed is 8.1.3.
However if you are seeing the 8.1.0 listed in Code Composer Studio -> Build -> Compilers that means it is available for use in CCS.
If you go to the properties of a project you will be able to select it. I am on a Mac so I can't show the C6000 compiler today but it would be here:
Regards,
John