This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Uniflash does not accept newer XDS110 firmware

Part Number: CC2640R2F
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

Both CCs and Uniflash newest versions

painful if you don't have the script for mass erase and need to use uniflash

May be Uniflash could accept newer firmware?

or may I just copy the CDS110 8.2 version over the 8.1 versions of Uniflash? will that work?

Best wishes

Ralph

  • Hi Ralph,

    This is a known issue where if the emulator pack versions between CCS and UniFlash are different. I filed an enhancement request to handle this better. Tracking ID: UNIFLASH-1285. 

    You may be able to manually update the UniFlash emulator pack version so that it is in sync with the CCS version. I'll experiment with this further and see if this is a viable option.

    ki

  • It seems I also have that page 30 verification error on top of the firmware update problem?

  • G.H. said:
    It seems I also have that page 30 verification error on top of the firmware update problem?

    For this issue, I'll reply to your original post