This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Both CCs and Uniflash newest versions
painful if you don't have the script for mass erase and need to use uniflash
May be Uniflash could accept newer firmware?
or may I just copy the CDS110 8.2 version over the 8.1 versions of Uniflash? will that work?
Best wishes
Ralph
Hi Ralph,
This is a known issue where if the emulator pack versions between CCS and UniFlash are different. I filed an enhancement request to handle this better. Tracking ID: UNIFLASH-1285.
You may be able to manually update the UniFlash emulator pack version so that it is in sync with the CCS version. I'll experiment with this further and see if this is a viable option.
ki