This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I developed the prototype using the design probided by the TI. Now I want to pragram the (MSP430F5132) present on the TIDA-010042.
How to use MSP-FET to program TIDA-010042?
is there cheap alternative to MSP-FET to pragram TIDA-010042?
kindly share suitable document and guide me.
thank you.
Hello,
Pls find below the steps how to program TIDA-010042:
1. Follow the MSP-FET connector pin definition page 21, see the link below
2. you need to some jump wires to connect the MSP-FET pins to the 5 highlighted pins below, see the design guide page 17
3. then you need to download and install CCS from the link below:
https://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html
4. then create a workspace in CSS import the TIDA-010042 SW: www.ti.com/.../tidcfd5
5. last compile and run the SW in CSS
Rgds
Lei
Hello,
Pls find below the steps how to program TIDA-010042:
1. Follow the MSP-FET connector pin definition page 21, see the link below
2. you need to some jump wires to connect the MSP-FET pins to the 5 highlighted pins below, see the design guide page 17
3. then you need to download and install CCS from the link below:
https://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html
4. then create a workspace in CSS import the TIDA-010042 SW: www.ti.com/.../tidcfd5
5. last compile and run the SW in CSS
Rgds
Lei
Hello,
to my knowledge, MSP-FET is the only way to program this ref design.
Rgds
Lei
One more thing I forgot to mention that for the step 1, you need to use the 2 wire JTAG setup in page 23 like the snapshot below:
And for step 2 the board can be either powered up by USB or the LDO, so you can select jump 3 to short the left two pins or right two pins.
Hi Sir, can i able to use any other MSP 430 launchpads for programming MSP430F5132 as MSP-FET is not availble in my region. because SBW protocol is coming with all MSP 430 launchpads. If so can u share the procedure for the same pls.
Hello,
I am not expert on MSP430, but you may try out with following steps:
see page 17, https://www.ti.com/lit/ug/slau533d/slau533d.pdf?ts=1646377845738
1. remove the jumpers
2. try to connect TST and RST and GND pins to J4 pin 2,3,4. Short pin 1,2 of J3. Power up the board with >12V.