This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi, can anyone help me out in a design of boost converter. the input voltage is 12-13.5 volts as output is 180 volts maximum output current is 150mA here i have achieved those but the problem is mosfet. The mosfet i am using SIHB11N80E which is greater specs. the design recommends Vds 250 volts and current 3 Amps but it is having 850 and 8 amps respectively. The mosfet is getting too hot when boost converter is on load either load is low or high. Help me please thanks is advance.Boost 180 @ 150 mA.pdf
Thanks a lot please give me the idea to choose the fet or what should be the solution so that i can solve this problem.
Garrett Roecker said:Garrett
Hi, what are the benefits of stacking a charge pump on the out put. Is it helpful to reduce the heating issue in the mosfet.
thanks in advance early reply is expected.