Other Parts Discussed in Thread: LM5118, LM5121
Tool/software: WEBENCH® Design Tools
hello,
Is the input and output polarity of lm5118 opposite? For example, can I input - 48V and output + 9V? As a buck boost circuit, it should support the opposite polarity of input and output. Why can my circuit output normal + 9V only when the input voltage is positive? Please help to answer, thank you!