This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352P: GIT and build errors

Part Number: CC1352P

Tool/software: Code Composer Studio

I just recently installed simplelink_cc13x2_26x2_sdk_2_40_00_81 and I'm in the process of porting my zstack project from simplelink_cc13x2_sdk_2_30_00_45.

In both cases I started with zr_genric_app.

It all builds correctly locally, but when I create a GIT repository and then clone that project I get build errors on the clone (so do my colleagues).  My guess is that I'm missing something in the GIT.

I used the instructions from "http://processors.wiki.ti.com/index.php/Source_control_with_CCS" to decide what to include/exclude.

Here's the build log file.

/cfs-file/__key/communityserver-discussions-components-files/158/global_2D00_build.log

Any thoughts?

- Bill