Texas Instruments (TI) MSP low-power microcontrollers support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search MSP low-power microcontroller content or ask technical support questions on value line, capacitive sensing, ultrasonic & performance sensing MCUs, as well as other MSP430™ MCUs. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI-Flash Smart Placement
Support for…
Other Parts Discussed in Thread: MSPM0L1306 Automatically set the LOAD_VALUE into TIMx.CTR via TIMx.CCCTL.LCOND is not work for period capture. It will have influence on "Period Capture" mode and "Combined Pulse Width and Period Time" mode. (Only use "Pulse…
Other Parts Discussed in Thread: MSPM0L1306 The timeout function on MSPM0G or MSPM0L UART can't reach ms level.
Here is an example to realize it based on 1 UART, 1 Timer, 2 DMA.
Here is the blockdiagram. The key point is that it doesn't use UART …
Part Number: MSPM0-SDK Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH ,
Important note for early MSPM0 customers
TI recently launched a new family of Arm Cortex-M0+ MCUs , including the MSPM0L series and MSPM0G series . These MCUs are accompanied by a…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: MSP430F5529 , UNIFLASH , ENERGIA , MSP-FET , MSP-FLASHER , MSP430F5528
Hi everybody,
I have a new MSP-EXP430F5529LP board, but I can't get it to work. Connecting the EVM to the PC via USB…
Part Number: CCSTUDIO-MSP
By default, CCS will detect the JTAG interface automatically based on the device and the debugger. However, you may want to manually change the interface type to 2-wire SBW or 4-wire JTAG. Currently, CCS does not allow you to…
TI is pleased to announce a new MSP430 compiler version 21.6.0.LTS which includes the following new features.
New features: - Generate CRCs over memory ranges.
- Enumerated type changes.
- Misra support deprecated.
- Performance improvement with BIC…
Part Number: MSP430FR2433
MSP housekeeping MCUs
A training series to help mix and match common analog and digital functions on a microcontroller.
Why housekeeping?
We know that you are looking for ways to make your board designs…
Part Number: MSP430F67791A Other Parts Discussed in Thread: EVM430-F6779 , , TUSB3410 , MAX3232 , MSP-ISO
Hello James,
sorry to bring back this discussion/queries again after several tries.Now looking at some alternate solution.
1) Could not able to get…
Hi E2E,
We have made a MSP430™ MCUs Development Guide Book to give some help to use MSP430.
Message from the editors:
This pocket reference is a valuable and quick guide to find all important MSP430 resources. This book serves many purposes – a…