Part Number: TI-RTOS-MCU
Tool/software: TI C/C++ Compiler
How can I control the placement of the "c_int00" program entry point with the TI Compiler for CortexM and C6x devices?
Part Number: DS90UB953-Q1
Hi,
I'm using a system with a n output of MIPI-CSI2. with one lane in 800Mbps, using the above Serializer and deserializer.
The spec only specified to latency of the GPIOs, is it possible to know the latency of both devices…
Part Number: MSPCAPTDSNCTR If you have a Microsoft Windows 10 PC with a 4K display and are working with TI's CapTIvate Design Center , Ultrasonic Sensing Design Center , or Energy Measurement Design Center software tools, than this post applies to you…
Other Parts Discussed in Thread: LMC555 , NE555 , LM555 , NA555 , TLC551 , SE555 , TLC552 , TLC555 , SA555 , CD74HC4060 , SN74LV8154 This FAQ covers mono-stable circuits using the LM555, NA555, NE555, SA555, and SE555 timers that are called LM, NA, NE…
Tool/software: WEBENCH® Design Tools
Over the years, we invested in numerous Flash-based tools supporting our analog and embedded portfolios. However, when Adobe announced it will sunset Flash by the end of 2020 and with browser makers also ceasing…
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TINA-TI
Tool/software: WEBENCH® Design Tools
Introduction :
WEBENCH® Power Designer is a free online power supply design tool, which creates customized power supply circuits based…
I'm confused with some of the TI SDKs usage of POSIX in their examples. For example, I see pthread_create all over the place. Is POSIX usage required or optional?
Other Parts Discussed in Thread: AWR1243 , DCA1000EVM , AWR1243BOOST , AWR2243 , AWR2243BOOST , TIDEP-01012 , UNIFLASH Q1. mmWaveLink_example usage/porting on External processor
MmWaveLink_example provides reference code to control AWR1243/P over SPI…