Part Number: TIOL1115 Other Parts Discussed in Thread: BOOSTXL-IOLINKM-8 , TIOL1125 , Tool/software: Hello, Is there anyway we can use your io-link stack with a headless build system? Or it's only available on your IDE?
Hi Dmitry, in case it helps for this project or in a future project.
- You mentioned looking for IOLink in sysconfig. For IOlink we had a booster board which sits on top of AM243x LP, so configuration is done through GPIOs (different Channels TX/RX). …
Hello Tech 00,
The WAKE pin is an output pin and is only used on the Device side of the IO-Link cable. It can be left disconnected when used in a Master application.
If the Device's CQ driver is enabled and the Master needs to take control of the line…
Hi Joseph,
Yes, TI has developed a solution using the Sitara LP-AM243 LaunchPAD and an 8-port IO-Link Master BoosterPack board (BOOSTXL-IOLINKM-8) that uses the TIOL112 for the IO-Link PHY and this board is in the final stages of our inventory stocking…
Part Number: BOOSTXL-ADS7841-Q1 Other Parts Discussed in Thread: ADS7841 Tool/software: Hi,
I am currently working with the ADS7481-Q1 EVM ( BOOSTXL-ADS7841-Q1) and have encountered some difficulties in obtaining accurate ADC values.
I have interfaced BOOSTXL…
Hello Issa,
The register (REC_LENGTH) data from address 0x22 has been been verified to be 0x19 (as above). P1_REC is 8.192 ms , while P2_REC is 40.96ms. The unwanted data occurred at 6.4ms ~8.192ms.
Beforehand, I had checked the following:
1a) Use BOOSTXL…
Part Number: MCF8329EVM Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM , LAUNCHXL-F28069M Tool/software: Hello All. I am creating a drone esc project from scratch and would like to utilize the mcf8329 to do so. I am having issues running the MPET algorithm…
Part Number: BOOSTXL-3PHGANINV Hi, I received two boostxl-3PhGanInv boards from a customer to use with two launchpadxl F28069M boards. When going through SLUUBP1A, the document suggests that there are 5 source files provided with the EVM software package…
Part Number: BOOSTXL-TPS650861 Other Parts Discussed in Thread: IPG-UI Hello,
In Step 8-1 of paragraph 4.4 (swcu190.pdf) is directing me to “Device Control Programming tab” … I don’t see that tab on my screen.
Regards!
Hello Taimur,
Thanks for posting to the sensors forum!
I wanted to ask if there is any way to check the correctness of UART communication with PGA460 similar to Command 0 which is used to test PGA450 UART communication.
There is no command 0 on the PGA460…