Hi Carlo,
Yes, we do have some parts that support your requirements.
CD74HC4067 and CD4067B are two recommendations. You can also find them and some other parts in the device selection tool here .
Please let me know if you have any questions.
Thanks
Sa…
Other Parts Discussed in Thread: CD4067B Hi, team
Could you please help me select a specific part number in multiplexers? here are the requirements.
1. there are 10 input signals which includes digital signals , 10V analog signals and a 5V,10Khz signal…
Part Number: MUX506 Other Parts Discussed in Thread: CD4067B Hi,
I could not find a real answer to my question in the datasheet.
I would Like to use the IC in an application where 3.3V and 5V are mixed.
The analog Voltage is between 0V to 5V and the voltage…
Amil,
You could use something such as the CD4067B 16:1 Analog MUX : www.ti.com/product/CD4067B .
Would this be an acceptable alternative? You will control this with four digital address bits from the central uC.
A block diagram of the interface bus would…
I am getting 0 sometimes.
I even get higher values than expected sometimes.
The input analog signal that I give ranges from 0-1V.
To explain what I am exactly doing:
I have units(DUTs with fuse) connected to the multiplexer input lines.
I have attached…
Other Parts Discussed in Thread: CD4067B , TS3A44159 , TS3A27518E , SN74LV4051A , SN74CBTLV3251 , CD74HC4067 Could you recommend analog MUX with 1.8V operation?
12 inputs go into 1 output. one chip solution is ideal. Discrete solution is acceptable.
Part Number: CD74HC4067 Other Parts Discussed in Thread: CD74HCT4067 , , CD4067B , CD74HCT4051 , MUX506 , MPC506 , MUX508 The customer is working on a design that has a lot of current and feedback loops they feed into an ADC.
They use a lot of MUXes in front…
Hi David ,
Can you consider CD405xB or CD4067B devices ? They are single 8 Mux devices or 16 Mux devices .Variations of these can be done for a differential configuration to be used in applications . They are available in DIP format for through hole insertion…
Other Parts Discussed in Thread: CD4067B I am currently a senior, working on my senior design project.
I need to pick a DSP developmental board/starter kit.
The application is a "real time" spectral analyzer for 20-30 analog channels. I have…