Other Parts Discussed in Thread: MSP430FR5739 , L293D , MSP430G2553 #include <msp430fr5739.h>
void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer _delay_cycles(1000000);
// Initialization of the port pins of MSP430G2553 - P1.5 is connected…
Other Parts Discussed in Thread: L293D , DRV8835 Hi ,
I am trying to run 4 Stepper Motors from a Micro Controller, Instead of using uC's GPIOs ,
I am thinking of using 4-16 Demultiplexer, One possible way is to use 4* 1-4 Demux with shorted address…
Other Parts Discussed in Thread: L293D , L293 I have got a MB PM35S-048 motor and I want to build a Knetic Energy Recovery System. The motor is drived in printers by L293 or L293D, but the driver only control the direction of rotation, but when the motor…
Other Parts Discussed in Thread: L293D , DRV8844 , DRV8829 Hello,
My name is Seth. This may sound silly but here goes it. I am making a web based controlled or WiFi keyboard controlled mower for goofing around. I wanted to learn more about robotics and motor…
Hello Sai,
I have tried the same code with a different motor driver IC, the L293D, and it's working fine. Seems to me that the DRV8870 is the problem. I have connected the ISEN pin directly to ground, and the VREF to +3.3V. The DRV8870 seems to be interfering…
Other Parts Discussed in Thread: L293D , CODECOMPOSER , MSP430G2553 , L293 hello,my task is DC motor control in CODECOMPOSER by using msp430 ,model of G2553 and the target is making the motor in two direction,forward and backword also by using Pwm to turn…
Robert,
Thanks. I have no idea what a J-Link is. I will check and see if I can get one.
As I replied previously, I am using a L293D to drive the stepper motor. Next step the data transmission...
The problem is very simple. Your L293D is powered at 5V. AM335X I/O pins in Beaglebone are powered from 3.3V and are NOT 5V tolerant. You must use level shifters when you interface to any voltage different from 3.3V.
You can safely assume that your processors…
Other Parts Discussed in Thread: L293D Hello Guys. Guys I am facing some issues regarding the integration of my TIVAC TM4C123G Launchpad with active PIR Sensor. Here is my code. There is no output at all on pin 2 PE2. even I checked the PIR output which…
Other Parts Discussed in Thread: L293D , MSP430FG4618 Sir,
I am a member of TI INDIA ADC Contest.I would like to know, how to interface apr9600 voice recorder and playback kit with MSP 430. I would like to know is there any requirement of coding and test…