Part Number: BQ27Z746 Other Parts Discussed in Thread: BQ-BATTERY-PROGRAMMER-SW , MKST-3P-ALT-EV2300 Tool/software: Hi,
Which BQ-BMS-PROGRAMMER-SW.exe file should i use for BQ27Z746 when programming golden image using MKS-SAI-001?
I tried with Prog27z5…
Part Number: MSP430F5510 Tool/software: I've implemented I2C master based on I2C examples source code. It works OK except one thing: when I make reset via debugger during I2C operation (for ex., on breakpoint inside interrupt processing), SDA remains…
Hi,
1) Yes, technically multiple BQ76907 can be connected to the same I2C bus.
2) You can change the I2C address after power up, refer to the TRM for more details https://www.ti.com/lit/ug/sluucj0/sluucj0.pdf .
The I2C device address (as an 8-bit…
Part Number: BQ25898D Hi TIer
My customer have find a fault chip of BQ25898D in mass production.
The chip pin impedance did not change significantly. and BQ25898D could not communicate and also no output (0V at SW, SYS, PMID). We suspect internal…
Hi Jared McArthur ,
Jared McArthur said: Do you have any thoughts on this suggestion?
We suppose linux sysfs is more convenient since we need to interact to other SW module for HW validation, status check, etc.
Thanks
Part Number: MSP432E401Y Tool/software: Issue:
We have tried shoring the I2C channel4 CLK to GND to replicate the scenario where the I2C communication link is broken between the MCU and Slave. Upon testing the scenario, we have observed that, once the…
Part Number: TMDXIDK5718 Tool/software:
While checking the UBOOT command, it suddenly hung up and the TMDXIDK5718 stopped working.
Pressing the RESET SW did not restore it, and neither did unplugging and plugging in the 5V power.
U-BOOT will not…
Hi Daniel,
Please use this link to submit your request for access of the TAS5805 device app. Once it is approved, you should be able to see the app popping up on your PPC3 after logging in... right beside I2C master tile.
https://www.ti.com/drr/opn…
Hi Kadeem,
Thanks for your response.
Our requirement is All output will be 100MHZ LP-HCSL only.
As per below image says if HW_SW_CTRL pin is HIGH by default factory programed will be 100 MHz LP-HCL, with XTAL 25 MHz input. Our requirement match…
Thanks for your kind reply Michael,
May you please confirm me the default battery charging current without i2c control and default SW output voltage and current to load.
I have checked in the datasheet, that default current is 1A and output voltage…