Part Number: LMV321-N-Q1 Other Parts Discussed in Thread: LMV321 , LMV321A Tool/software: Good evening,
I'm trying to simulate a buffer circuit with an LMV321 in PSpice for TI (see first picture), theoretically I shouldn't be respecting the common mode…
Part Number: LMV321-N Tool/software: Hi,
We are using LMV321N for our design, as differential amplifier, for error calculation we need the output offset voltage which couldn't find in the datasheet.
we are awaiting for your reply at earliest.
Thanks…
Part Number: LMV321-N Other Parts Discussed in Thread: LMV321
Tool/software:
We have a specific case that we need some clarification.Normally, our circuit is functioning with 3.3V on Inputs and 3.3V on Outputs, but we have some units where the component…
Part Number: LMV321-N Dear Team
We are currently performing an FMEDA for our VCU project. To complete our analysis, we urgently require the following information:
FIT (Failures‑In‑Time)
data Failure mode distribution / percentage breakdown
…
Part Number: LMV321-N-Q1 Other Parts Discussed in Thread: AMC1311-Q1 , AMC1311 , LMV321 Hi TI expert,
May I know how to judge the Vout tolerance if we short the " right side " of the R218 & R219 together in the below application? We add a 0.5V offset…
Part Number: LMV321-N Other Parts Discussed in Thread: TLV9001 Hello:
LMV321M5X/NOPB is used on the customer's motor motherboard, the main purpose is to monitor the temperature through the output voltage of the chip. During the test, there were several…
Part Number: LMV321-N-Q1 Other Parts Discussed in Thread: OPA2365 , LMV321 , TLV6001-Q1 Hi,
I'm used LMV321-N-Q1 for PFC input voltage feedback.
OPA supply voltage is 3.3V.
When opa input is 110v, the output voltage be clamped arond 2.06v.
…
Part Number: LMV321-N-Q1 Other Parts Discussed in Thread: LMV321 , ADS7052 Hi Team,
LMV321IDBVR is used in the voltage monitoring circuit, customer encountered a problem in the test: When testing at low temperature of -40 degrees, the monitored voltage…
Part Number: TDP142-Q1 Hi Teams,
Does this pin swap mean that, within the TDP142-Q1, the DP differential input pins P and N can be swapped? If so, can the P and N pins of the DP differential inputs for D0, D1, D2, and D3 all be swapped? It should not…