Other Parts Discussed in Thread: MSP430F5636 This is a follow-up post to a previous post . I've also submitted a request to TI's MCU group but no answer.
I can't get any of the USB Developer Pkg example programs to enumerate. I've tried CCS on…
Part Number: MSP-TS430PZ100USB Tool/software: Code Composer Studio OS: XP
CCS version: v5.3
Device: MSP-TS430PZ100USB of the MSP430F5636 and MSP-FET430UIF
Hello,
I recently using MSP-FET430UIF programmers for my device, my code uses " Blink The LED " in CCS…
Hi Thomas,
My input voltage (input signal to the op amp) can vary only from 0V to 3.3V (using the DAC from the MSP430F5636). The supply voltage for the op amp is 100V (V+) and GND (V-).
Will it help if I use first stage amp (with low gain) and then go for…
Hi Leonard,
I believe we have a solution with the MSP430F5636 and CC2520 from a 3rd party. Not sure about a CC26xx solution yet.
WHART uses the IEEE 802.15.4 -2006, (so it is a IEEE compliant PHY PDU with maximum payload of 127 bytes.
It is a secure…
Other Parts Discussed in Thread: MSP430F5636 Using MSP430F5636 and TI-RTOS 2.1.0.03. In order to ensure that an I2C bus never gets blocked I reset the I2C module if the UCBBUSY bit stays high for 10sec. To do this I use the following code:
//This function…
Hi Thomas,
TA0CTL is one of the registers defined for Timer TA0. Not every MSP430 member has Timer TA0 implemented in hardware, in this case this symbol is not defined. Some may have only one Timer A, in this case symbol TACTL is defined instead of TA0CTL…
Other Parts Discussed in Thread: MSP430WARE , MSP430F5636 Hello everybody,
I´m getting this error:
s.knl.Event: create policy error xdc.runtime.Error.raise: terminating execution
when calling to the Event_create function.
I´ve been reading the forum…
Other Parts Discussed in Thread: MSP430F5636 I been trying to trouble shoot a weird problem on our custom PCB. The project is one of our military SPIRs.
I'm using the MSP430F5636 (100pin), MSP-FET430UIF programming/debug in SBW mode and CCSv6.
The…
Other Parts Discussed in Thread: MSP430F5636 I am working with the MSP430F5636,
I was wondering if it possible to use the port mapping module (port 2, P2MAPx) to remap for analog input or remap to DAC out pins??
If it can use the analog input, how do I…
Other Parts Discussed in Thread: MSP430F5636 Greetings... I'm working with a MSP430F5636 and I'm using the Battery Backup system. The 5xx/6xx Family User's Guide clearly states that if you're not using the Battery Backup system that VBAT should…