Part Number: SN74LVT125-EP Other Parts Discussed in Thread: SN74LVT125 , SN74LVTH125 , SN54AC244-SP , SN54LVCH244A-SP , SN74LVC2G126-EP I need to drive a SPI clock bus signal from a microcontroller (with low drive strength/high output resistance) to 12 devices…
Part Number: SN74LVT125 Dear all,
my AA is using the SN74LVT125 in the following condition:
Vcc 3.3V
Vin (1A,2A,3A,4A) = GND
1OEn, 2OEn, 3OEn, 4OEn driven by FPGA (GND, 3.3V levels)
Output 1Y, 2Y, 3Y, 4Y connected all together to Pull up resistor to 5…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LVT125 , , SN74AVC4T245 , LSF0108 I want to always sense the input from the bidirectional line to the input pin 1 through voltage translator. The voltage translator is used because the logic level…
Other Parts Discussed in Thread: SN74LVT125 Is this information available for the SN74LVT125?
1. What is the typical threshold voltage between the 0.8 and 2 V switching levels?
2. What are the variations with temperature?
Part Number: SN74LVC125A Other Parts Discussed in Thread: SN74LVT125 Hello team,
I'm looking for a good 3 state solution which has both partial power down and HIZ during power up features. I consider either SN74LVT125 or SN74LVC125A. I can find equipped…
Yes current sink ic is SN74LVT125.I have connect the output of DS90LV048A TO SN74LVT125.AND SN74LVT125 INPUT CHARACTERISTICS IS SAME AS OUT WAVE FORM AS I HAVE ATTACHED PREVIOUS.
You get identical characteristics by staying in the ABT family. There is no four-channel device with a single OE , but you can use the SN74ABT125 and route the same signal to all four OE s (this is no problem with high-impedance CMOS inputs).
The only alternative…
Hi Lou,
It will definitely work, but as i mentioned, performance will be compromised especially jitter.
I was able to do a quick search and did find a device which might be promising: https://www.ti.com/lit/ds/symlink/sn74lvt125.pdf?ts=1597731648386&ref_url…
Other Parts Discussed in Thread: SN74LVT125 Hi, Would like to know about the Environment (Industrial/Automotive) in which SN74LVT125PWR IC can be used.