Part Number: DRV8350S-EVM Other Parts Discussed in Thread: TIDA-01629 Hi Team,
After referring to TIDA-01629, the customer used this board to control the motor and found that the motor could not rotate. During the program debugging, it was found that the…
Hi,
NT means Net-tie. This is just connected/shorted. The reason for this net-tie is to allow power nets of different names to connect directly without the design environment having DRC errors.
e2e.ti.com/.../drv8350-what-is-effect-of-net-tie-in-tida-01629…
Mark, apologies for late reply,
Mark Philip Felipe said: So is it possible to program the R5F and M4F cores of the SK-AM64 kit or not
yes it is definitely possible to program R5F & M4F cores of the SK-AM64.
Mark Philip Felipe said: Also CCS does not…
Hello Art,
You are not going to find an evaluation module that can drive that level of power (>1kW) off the shelf. None of our EVMs are designed to plug and play with an encoder.
The best you can do is use an EVM which has lower power and no encoder…
Part Number: DRV8323R Other Parts Discussed in Thread: TIDA-01629 Hi,
I have my own design with the DRV8323RS see also previous case CS0271338.
I went to change the PCB, the question is do you have on this time a driver IC with the possibility bloking…
Song,
This device is the extended temperature version of the DRV8353 so any of the reference designs that apply there can also be used here:
http://www.ti.com/tool/TIDA-010056
http://www.ti.com/tool/TIDA-01629
Regards,
-Adam
Hello,
The first motor seems like it has significantly higher power than the second motor.
Please take a loom at the C2000 microcontrollers for motor control, these devices will be able to interface with your encoder and implement FOC to drive the motor…
Part Number: THVD1550 Other Parts Discussed in Thread: TIDA-01629 Hi Team,
My customer is using THVD1550 in their design and have some questions about the external circuit of this part.
According to the TIDA-01629 as below picture:
1. Does R76, R77 has…
Part Number: INA240 Other Parts Discussed in Thread: TIDA-01629 ,
Hi,
I am using a INA240A1 in a similar configuration as the in the TIDA-01629 Reference Design: http://www.ti.com/tool/TIDA-01629 Unfortunately I see some coupling between channels sampled…