Other Parts Discussed in Thread: ULN2003A , TPL7407LA , TPL7407LA-Q1 Hi,
I'm designing a board and looking for a Low Side Driver/Output so I can sink the signal. I'd like to sink a load powered by a 12V supply.
Thanks,
Kash Olia
What is the minimum voltage at which it must switch on? What is the maximum voltage at which it must switch off?
As far as I can see, there is no single chip that can do this. I'd suggest six comparators and a TPL7407LA-Q1 (switching to ground).
Part Number: SN74LVC1G17 Other Parts Discussed in Thread: SN74LVC541A-Q1 , TPL7407LA , SN74BCT25244 Cross to PN: SN74LVC1G17QDCKRQ1
https://www.ti.com/lit/ds/symlink/sn74lvc1g17-q1.pdf
We are looking for a part that has an output current capability of …
Part Number: ULQ2003A-Q1 Other Parts Discussed in Thread: TPL7407LA-Q1 could ULQ2003A-Q1 be used in 24V automotive system? is there a success story? thanks.
Part Number: LP2901-Q1 Other Parts Discussed in Thread: TPL7407LA-Q1 , , TLV1701 Hi team,
My customer is thinking to develop automotive interior LED lamp, multiple LED shall be used in this application.
I would like to promote TPL7407LA-Q1, which is low…
Part Number: TPS22810 Other Parts Discussed in Thread: , DRV103 , TPL7407LA , TPS1H100-Q1 , DRV8873-Q1 , DRV8801A-Q1 , DRV8872-Q1 Hi Team
My customer wants to control 6 ~ 7V / 1A power at 20khz.
Is the TPS22810 capable of 20khz PWM control?
If not, please…
Part Number: TPS4H160-Q1 Other Parts Discussed in Thread: ULN2003A , TPL7407LA Hello,
Do we have a GND/OPEN (Low Side Driver) version similar to the TPS4H160A?
Regards,
David
Other Parts Discussed in Thread: DRV2510-Q1 , DRV2511-Q1 , DRV2625 , ULN2003A , TPL7407LA I have a 24V DC Solenoid I bought from Digikey. its a push pulse, and i want to drive it both directions one to set it one to release it. I've seen tons of options, …
Part Number: TPS22810 Other Parts Discussed in Thread: TPS1H000-Q1 , TPL7407LA Hi TI Experts,
I plan to use TPS22810 as load switch to drive a relay for power supply sequences.
Can TPS22810 able to drive an inductive relay?
The load relay characteristic…
Part Number: TPL7407LA Other Parts Discussed in Thread: TPL7407L , Hello guys,
One of our customers is considering to evaluate TPL7407LA released May/2017 because it seems that the device is improved version of TPL7407L. On TPL7407LA datasheet, they knew…