Part Number: DRV8243-Q1 Hi team,
My customer is evaluating DRV8243SQRHLRQ1 in their project and met below question, could you please help review and give some comments? Thank you!
When the customer debugs the DRV8243S-Q1, the motor will operate normally…
Part Number: TDA4VH-Q1 Hi TI Experts,
Customer is trying to use MCU4-0 to implement AUTOSAR & MCAL drivers.
However, when we look at the supported cores for the MCAL drivers, it seems only MCU1-0 & MCU2-1 are allowed shown below.
May I know could…
Part Number: ADS131B26-Q1 Other Parts Discussed in Thread: ADS1256 , ADS131M06 , ADS131E06 Tool/software: Hello E2E Experts,
Good day.
Basically what I'm looking for is a product recommendation, an ADC that measures a voltage between 0 and 3.3 V, that…
Part Number: TXS0108E-Q1 I am trying to use part #TXS0108EQPWRQ1 to shift signals from 3.3v to 5v. I have VCCA connected to 3.3v and VCCB connected to 5v. OE is connected to 3.3v as well to always enable the LS. I am noticing that the b side outputs always…
Part Number: AM2634-Q1 BU team,
I am asking this issue for my customer, it is an urgent case. Please put into high-priority list.
Customer uses core 1-0 as lockstep core and implements FuSa diagnostic functions. Recently they added some codes (just some…
Part Number: TDA4VEN-Q1 Other Parts Discussed in Thread: TDA4VM Tool/software: Hi TI experts,
SDK: ti-processor-sdk-rtos-j722s-evm-09_02_00_05.tar.gz
I run the graph in pipeline mode.
It show error:[C7x_2 ] 10386.070921 s: VX_ZONE_ERROR:[tivxMemBufferMap…
Part Number: DRV3946-Q1 Tool/software: Hi. I am searching for an optimal driver that controls the opening and closing of a small 24V 500mA solenoid valve and wondering if the driver can handle that device at maximum 24V and 12mA
Thank you so much b…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH Hi TI Experts,
Customer is upgrading from SDK9.1 to SDK9.2 on TDA4VH.
All of their SW components have upgraded to SDK9.2 successfully, but the MCU1-0 firmware seems have some problems.
Currently…
Part Number: DP83TC814S-Q1
Hi Expert!
We are using DP83TC814S-Q1 in our custom HW.
Current we are facing - PHY is not found on the MDIO bus issue.
qcom,emac: MDIO device at address 0 is missing
.
We have checked the DP83TC812 Troubleshooting Guide
…