Hello Karthik,
We saw in another thread ( https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1409311/tda4vh-q1-does-the-tda4vh-chip-support-mcu-only-mode-function) that MCU-Only mode is not supported in SW SDK J784S4.
Anyhow, we are…
hi
as per hardware requirement we are changing the external RTC chip to PCF8583,hence i write the code for same as below ,but I2C interrupt is not generated ,kindly correct me in code.
#define SlaveAddress 0x51
void InitI2C(unsigned char eeprom_i2c_address…
Other Parts Discussed in Thread: TAS3251EVM Tool/software: I need to PPC3 to communicate with the TAS3251EVM, but in the PPC3 all I have is the I2C Master app. How do I install the TAS3251EVM app in the PPC3 (running v3.2.1), which I have dowloaded ( https…
Part Number: TUSB422 Tool/software: Hi, Ti Team
Our SW team says that the stack structure of the source provided can only control one TUSB422.
I2C Channels are connected individually and I want to control 4 TUSB422.
Isn't it possible to control four…
Hi Thom,
We don't have specific software example for interfacing with BOOSTXL-EDUMK11. However, there are several examples in TivaWare SDK. Please download the SDK from https://www.ti.com/tool/SW-TM4C . You can find examples in the below directories…
These scope shots were taken at relatively (but not exactly) the same time. The large I2C transaction you see on the far left is the same in both instances, this is the mode table being written. In both the good and bad cases you see a bit of I2C activity…
The issue is quite odd, even without the SW inductor circuit the amplifier does not output anything. The register being set to 0x00 twice was gathered from the example MCU integration and setup code I mentioned earlier, changing this does nothing unfortunately…
Hi Jaehoon,
We have 3 I2C EEPROM SW Examples as well as I2C EEPROM drivers within C2000Ware that showcase how to communicate between I2C and EEPROMs in different ways.
Best Regards,
Aishwarya
Part Number: MSP430F5525 Dear team,
A customer has the following request.
One of their old products reported a NACK issue in the field; it turns out to be a FW bug caused the I2C to reset.
They solved the problem but they would like to know how long…
Hi Jochem,
Thank you for reaching out via E2E. Please see my comments below.
Jochem van Kranenburg said: If I understand correctly, we can make the OTG pin high and set the OTG_CONFIG bit through I2C to disable and enable the output on PMID. What can I…