Part Number: CDCDB800 Hi,
In our design x16 lane PCIe is splitted into 4x4 lane ports at endpoint, so we need a clock buffer.
I opted CDCDB800 ,since each x4 should support dual port feature, thus x16 lane to 4x4 , will work as 8x2 lane, thus 8 REFCLK…
Part Number: CDCLVC1103 Hi,
We have placed an oscillator close to the ASIC, but we are considering using multiple ASICs in the future. I am considering whether it will work fine with just one oscillator for multiple ASICs, or whether it would be better…
Part Number: ADS131M08 Hi team,
For the source-termination resistor placed at the clock buffer, do you have any specific value suggestions or reference design?
Thanks!
Regards,
Ivy
Hello,
I'm looking for an octal inverting clock buffer. 8 inputs, 8 inverted clock outputs, that can run at up to 20MHz and have a propagation delay of less than 10ns.
I'm thinking the
SN74LVC540A-Q1
will do the job. Are there any better suggestions…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: TXU0102 , SN74LVC2G34 Hi Team,
can the SN74LVC2G07DRY be used to buffer two clock lines that are 5 V level and to convert them to 3.3 V as well?
What is the skew between the two devices? E.g., if one…
Part Number: TMDS243EVM Other Parts Discussed in Thread: AM2432 , DP83869 The EVM shows additional clock buffer circuits for the PHYs. Customer does not see the need for additional clock buffers because the AM2432 has the clock outputs on A18 and V13 (ALX…
Part Number: LMK1D1204 Other Parts Discussed in Thread: LMK1D2102 , CDCE6214 hi,
customer is searching a clock buffer with below retirements. any suggestions?
supply voltag:1.8v;
Input signal : single-end 125Mhz LVCMOS;
Output signal: differential…