This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Pins 2, 4, 5, 7 are listed as VDD1 terminals.
Do I need to connect 3.3v to these pins vs
These pins are connected to Vdd2 pins inside the package
Thanks, archieb
abarter@allegromicro.com
Hi Archie,
yes, all VDD pins must be connected and all with individual supply voltage decoupling caps. Only by this the parasitic inductances can be kept at a minimal level and optimum performance can be achieved
See the datasheet for further information.
Kai