Other Parts Discussed in Thread: INA238, INA228, SYSCONFIG, INA240, INA190
Hello,
I'm trying to get a 4-20 mA current to read through the INA226 but am not having success thus far.
I do get readings, but they dont correlate with applying pressure on the sensor thats connected.
Details:
Shunt: .002 ohm
Max expected amps: <1 as it will be in the 4-20 mA range.
Sensor will be powered by a 12v source.
I've used a current to voltage converter module that has worked fine to ensure the problem wasn't with the sensor.
I think it has to be with the programming but not completely sure.
So far I've turned off averaging, because right now I'm just looking for a range of values as I apply pressure to the sensor, to verify if anything works.
Even though I'm using a small current - wondering if I need to set the max amps higher. I'm not sure if its max amps I expect, or a calculated value.
Anyway - all help is appreciated, thanks!