Other Parts Discussed in Thread: OPA2613, OPA593, OPA541, OPA1622
Hi Experts,
Our customer is looking for Precision Op Amp with tight accuracy requirements. Please see details below:
- Vos<1mv and low noise that can source 100mA to a 50 ohm load.
- The output reference uncertainity (u95%) shall be < +/- [0.1% FS] which is basically noise around the mean
- The output reference static uncertainity (u99%) shall be < +/- [1% FS] which is basically offset of the mean
- The output temperature coefficient uncertainity (u95%0 shall be < +/- [0.01%FS/deg C]
- The output drift uncertainity (u95%) shall be <+/-[0.1%FS] over 10 years
- I have to put a 50 ohm series termination on the output which goes to a coax cable and a 50 ohm load. I need to source current for that
Would you kindly help? Thanks in advance.
Regards,
Marvin