Part Number: OPA549
Other Parts Discussed in Thread: TINA-TI
Hi,
My OPA549 Op Amp keeps blowing when configured as an inverting amplifier. I have a 700 Hz, 20V low power input, and I want to generate an inverted, 700 Hz, high power output. My gain is set at 1. OP Amps are powered from a single supply (24V battery).


Any ideas? Could it be the 12V supply going into the non-inverting input? When the OP Amp blows, it generated a sinewave output that is clipped on the position side.
Thanks.