This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir,
Kindly provide the Voh(min),Voh(max),Vol(min),Vih(min),Vih(max),Vil(min),Vil(max) of TLC374IDR differential comparator.
With regards,
Arya
Thank you, Kai and Clemens, for your inputs.
Arya,
Thank you for the post. In addition to Clemens's comments, please refer to the datasheet here: Quadruple Differential Comparators datasheet (Rev. C). VOL is about 150 mV at IOL = 4mA at room temp.
-Chi