Part Number: OPA2675
Other Parts Discussed in Thread: OPA2670, STRIKE, OPA2677
Hello E2E Experts,
Good day.
I am developing a laser communication system. For the laser transmitter, we have split the project into the laser bias controller and the laser modulator. We are now developing a laser modulator.
1. I would like to know if Texas Instruments has any design/application notes for creating laser modulators with a high current output (1.5A) and a 5V output with a frequency of at least 25MHz.
2. We have reviewed several different op-amps with a high gain bandwidth product and high output current:
a. The OPA2675 has a GBP of 730 MHz and a max output current of 1000mA. Our concern is Figure 8-5, where it would appear that it may not be possible to achieve both 5V output and 1000mA of current simultaneously and stay within 2W dissipation. Will the chip limit the output to prevent it from reaching both 5V and 1000mA? Could we use two or more of these chips in parallel to reach a higher current output?
b. The OPA2670 has a 1.4GHz GBP and a max output current of 700mA. To reach 1A output, we are considering using two of these op-amps. How can we utilize both of these op amps in a circuit to create a laser modulator capable of 1A output?
c. As our laser diode heats up, the forward voltage of the diode will change. Are there any methods of accounting for this (in addition to adding a thermoelectric cooler)?
Regards,
CSC