Part Number: PGA309
Regarding programing set points for the "USB-DAQ EVM" when calibrating the PGA309.
I have been using the "USB-DAQ EVM" to calibrate the "PGA309" signal conditioning IC for use with a strain bridge with good success. I have used the "USB-DAQ EVM" successfully as a single unit calibrator and as the brain of a Multi-Cal system calibrating up to 24 PGA309's. We have purchased 8 of the "USB-DAQ EVM" boards again with good success. About 6 months ago one of the "USB-DAQ EVM" units started to insert a slight offset to the calibration point. Enough to cause unacceptable calibration errors. This was a unit used only for testing. Not sure to the cause, I replaced the onboard AtoD thinking there was a problem with it. Then I reloaded the software. The offset persisted and the software reload didn't help. To continue using the unit for calibration experiments, the offset was incorporated into the set point to get a better calibration. (The offset was about .093v high at the F.S. or 4.593. So the set point was reduced by .093 or 4.407. it wasn’t perfect but close enough for my testing.) When I used a different "USB-DAQ EVM" the offset went away. I believed this to be a one off and didn't pursue it further.
One month ago a similar offset started occurring with our 24 channel calibrator. Note this unit had previously been working fine for some time. This is a serious problem as it is part of our production line. Note that the Multi-Cal system no longer uses the "USB-DAQ EVM" onboard AtoD as a voltage measurement it uses the HP34401 multimeter. The symptom is still the same.
Has there been any other problems like this? Do you have any ideas how to fix it?
I have attached some images showing an independent meter monitoring the actual set point and the indicated voltage in the software. They are clearly different and I have used many other meters to check this. They all show the same offset. This offset is real and it is programed into the PGA309. Again, if I use a different "USB-DAQ EVM" the problem goes away.