This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
For the LMH32404 is it possible to connect VCC to zero volt and GND to -3.3V.
This is in order to amplify input currents that are sourced (not sinked) from the photodetector
Thanks,
Yuval Minster
Applied Materials
Hi Yuval,
The LMH3204 can be used to amplify sourced input currents from the photodetector with VCC set to 3.3V and GND to 0V.
Three things to note when sourcing an input current:
Please refer to Section 7 of the data sheet for more details on this or let me know if you have any other questions.
Thanks,
Nick