Part Number: VCA822
Hi, I'm using VCA822 with cascade structure. Therefore, I could not give the right results of the simulations. With this structure below,

After U1, Instead of 1V, I get 724.8 mV as seen below.
After U2, I must get 2V if input 1V because I set the gain voltage as -0.6V (2V/V gain). Or for 724.8 mV, at least I must get approximately 1.5V. But I get 1.076V as seen below.

Why this results are so wrong? Am I making a mistake? Could you help me?